|
|
 |
 |
 |
 |
| |

|
Hidekazu Oda
Senior Engineer
Advanced Device Technology Group
Advanced Device Development Dept.
Process Technology Development Div.
Production and Technology Unit
Renesas Electronics Corp. |

|
Takashi Hayashi
Engineer
Advanced Device Technology Group
Advanced Device Development Dept.
Process Technology Development Div.
Production and Technology Unit
Renesas Electronics Corp. |
Renesas has produce a prototype CMOS device incorporating technology that uses the implantation of fluorine in the substrate to overcome the problem of increased threshold voltage (Vth), which previously has been an obstacle to the practical application of HfSiON gate dielectric film. A prototype 8Mbit SRAM that uses this technology has been produced. Despite the fact that variation in the threshold voltage is a particular problem in SRAM devices, the 8Mbit prototype achieved full operation of all bits. |
| |
| Using fluorine implantation to improve carrier mobility |
| |
Advances in scaling have led to thinner gate oxide films, which, in turn, have caused increased gate leakage current due to the phenomenon of tunneling. To overcome this problem, high-k(high permittivity) gate dielectric films is required that are physically thicker than an electrically equivalent oxide film. However, combining a polysilicon (PolySi) gate with a high-k dielectric film results in pinning at high threshold voltage(Vth) by Fermi level pinning phenomenon, a problem for low voltage operation circuits. Renesas has solved this problem by implanting fluorine in the substrate. The new semiconductor process, which was described in IEDM paper 36.7, achieves a 0.2V reduction in Vth, an improvement of 33 percent or more over previous approaches.
Because of its lightness, boron for p-type gates can easily be diffused by annealing process. Diffusion of boron from the gate to the substrate across the dielectric film results in various problems, including degraded dielectric film reliability and increased fluctuation in the threshold voltage due to non-uniform boron profile at surface of substrate. Although it has been found that implanting fluorine in the gate actually promotes the diffusion of boron from the gate, the new results show that the boron diffusion can be suppressed by implanting fluorine in the substrate.
If boron implantation is used to control the threshold value, the threshold increases and the reverse short-channel effect is encouraged, which reduces the drive capacity. Use of fluorine implantation to control the threshold is effective for dealing with these problems. Also, if fluorine implantation is used to control the threshold, the boron profile remains unchanged and a low junction leakage current can be maintained.
A new discovery is that fluorine implantation increases hole that is p-type carrier mobility. Hole mobility is reduced when a high-k film is used; yet the use of fluorine implantation has the effect of improving the hole mobility. |
| |

Figure 1: Formula for fluctuation of threshold value. The EOT is the equivalent silicon-oxiside SiO2, film thickness that provides the same electrical characteristics as the actual film thickness used. Reducing the EOT causes the dielectric film capacitance to increase, and this results in improved transistor performance. Reducing the EOT also helps reduce the fluctuation of the threshold. Here L is the gate length, W is the gate width, N is the substrate concentration, q is the unit charge, ΦB is the internal potential, T is the actual thickness, ε is the relative dielectric constant, and the subscripts Si, ox, and x represent silicon, silicon dioxide film, and high-k respectively. |
|
| |

Figure 2: Effects of using a high-k film. A high-k film increases the current flow for nMIS, but decreases the current for pMIS because of reduced hole mobility. On the other hand, a high-k film reduces the substrate concentration and provides scope for adjusting the internal profile. By optimizing the "pocket" profile, a 14 percent improvement for nMIS and 50 percent improvement for pMIS was achieved. |
|
| |

Figure 3: Transistor V-I characteristics. Currents of 615nA for nMIS and 221nA for pMIS were obtained for a device with a 55nm gate length (equivalent to 65nm nodes). |
|
| |

Figure 4: Comparison with competing devices. The process technology developed by Renesas produces chips that have more current for both nMIS and pMIS than other devices. |
|
| |
| Obtaining full operation of all bits despite SRAM sensitivity to Vth fluctuation |
| |
A prototype 8Mbit SRAM produced using the fluorine implantation technology provided excellent results in terms of on/off performance (see Figure 2). As a device, an SRAM has both a short gate length and width. The narrow channel characteristics in the gate width direction are particularly important. The reverse narrow channel effect causes the threshold to lower and the leakage current to increase as the gate width gets narrower. Although this is an issue, excellent results were achieved for both nMIS and pMIS by using a high-k film, which has thick physical thickness for the same electrically equivalent oxide thickness (EOT). Specifically currents of 615nA for nMIS and 221nA for pMIS were measured for a device with a 55nm gate length, corresponding to 65nm node (see Figures 3 and 4).
The static noise margin (SNM) for the SRAM was adequate for practical applications and measurements confirmed the reduction in gate leakage. Despite the sensitivity of SRAM to fluctuation of the threshold voltage, all bits were verified to be fully operational. Moreover, test results showed a reduction in the fluctuation (scatter) of the threshold voltage (see Figures 5 and 6). |
| |

Figure 5: Vth fluctuation(Pelgrom plot). The high-k film decreases the fluctuation of the nMIS and pMIS thresholds. |
|
| |

Figure 6: Fluctuation in threshold value for each process generation. The threshold fluctuation increases with each successive generation from 90nm node to 65nm node and 45nm node. The results show that using a high-k film with 45nm nodes gives a threshold fluctuation similar to that of the SiON film used in a 65nm node process. |
|
| |
|
|
|