| 2-7 Characteristics of Instructions |
  |
This section describes the characteristics of instructions.
<Transferring immediate data to registers>
The 8-bit immediate data is contained in instruction code. When transferred
to general registers it is sign extended.
16-bit data and 32-bit data are allocated to memory.
This data has the displacement size of 8-bits, so it can be allocated from
the current program counter to 256 data area. If it is long word data it
can be allocated to the area of up to 1K byte from the program counter.
Therefore when a program is large it is divided to secure data fields in
between and programs will be connected by unconditional branching instructions.
The unconditional branching instructions include return instructions from
subroutines.
In the Renesas assembler data of any length can be described as immediate
but the assembly results are converted to PC relative.
<Address storage>
It is efficient to use the MOVA instruction to store 32-bit addresses in
general registers.
However, only R0 can be specified as the destination for a MOVA instruction.
<Conditional branching instructions>
For conditional branching instructions, when comparing data by specifying
conditions using CMP/cond instruction True or False will be displayed as
the resulting T bit, then the flow changes using the BT or BF instruction.
Data comparison is always done in 32 bits.
8-bit data is sign extended and compared with R0. Immediate data can be
compared to R0. Registers other than R0 cannot be used.
16-bit data is extended to 32 bits to be compared.
Signed data is sign extended to 32 bits with the MOV instruction, and can
be compared right away.
Unsigned data is compared after signs extended by the MOV instruction are
extended to zero.
32-bit data can be compared directly.
MOVA Symbol, R0
Signed 8-bit size displacement can be specified as the branch destination,
so BT and BF instructions can branch into up to 128 instructions as shown
in the diagram.
<Unconditional branching and subroutine calls>
These instructions branch using PC-relative addressing. Displacement is
used for specifying the instructions’ branching destination. Symbols
are usually used in programming.
These instructions specify displacement in general registers so branching
is possible in any memory space. Therefore it is possible to create position
independent programs (object programs that can be allocated to any position
in the memory map) in all memory spaces.
These instructions branch at absolute addresses. The instructions are executed
after storing the branch destination address as 32 bits in general registers.
These branch instructions are delayed branch instructions.
The instructions allocated to delay slots will definitely be executed with
the delayed branch instructions, so instructions should carefully be allocated.
Among conditional branch instructions, BT/S and BF/S are delayed branch
instructions.
<Procedure registration>
The stack area is not used to call subroutines. The procedure register stores
the return address. Because there is only one procedure register, save the
contents of the procedure register to the stack area to nest subroutine
calls.
<Multiply instructions and multiply/accumulate instructions>
The multiply instructions and multiply/accumulate instructions store results
in the MAC register.
This multiply instruction is a 16-bit x 16-bit = 32-bit operation. There
are also double precision multiplication and 32-bit multiplication. The
results of any of the operations are stored in the MAC register. The MAC
register has a 64-bit structure. This register is a system register and
is read using dedicated instructions.
There are word-sized and long word-sized multiply/accumulate instruction
operations. MAC instructions multiply between signed integers or between
fixed decimal data allocated to memory and add with the MAC register. It
is suitable for queue operations or filter operations.
In filter operations the calculation result may overflow and be changed
to the wrong symbol due to a calculation precision problem. Therefore the
MAC instruction makes it possible to saturate results when overflow or underflow
occurs by setting S=1 for the S (Saturation) bit of the Status Register
(SR).
<Division instructions>
For division 1-bit division instructions are repeatedly executed. The Div0
instruction prepares for division and the Div1 instruction executes just
the number of bits for division.
We’ll show an example of 16-bit division.
Division is performed after upper alignment is done to confirm it is not
division by 0.
Functions that are not in the division instruction are performed with other
instructions.
The DIV0 instruction initializes M and Q.
The DIV1 instruction outputs the quotient to the T bit.
The DIV1 instruction subtracts the previous T-bit quotient while it takes
the R1 dividend from the lower bit. It is easier to understand it as executing
subtraction and rotation with the T-bit.
The T bit of the last quotient remains the same so it will be added to the
quotient by rotation with the T-bit.
The upper 16 bits is data like a remainder. It can’t be used as it
is so it is 0 extended, and treated like the quotient.
Any CPU takes time for division. SuperH executes division by repeating 1-bit
division instructions and provides high speed response to interrupt requests.
<Dynamic shift>
There are instructions that allow free changes of shift volumes that use
barrel shifters and shift instructions that fix bit numbers. All of the
instructions operate within a single clock cycle.
<Privileged instruction>
Instructions that can have a critical effect on the system must be executed
in privileged mode. These instructions are called privileged instructions.
LDC/STC instructions except for GBR, LDTLB instructions to set MMU, RTE
instructions to return from exception handling programs and SLEEP to transfer
to low power consumption are privileged instructions.
If they are executed in user mode it will be a violation of privilege and
will be transferred to exception handling as a general invalid instruction
exception.
<Mode transition>
The CPU has 2 operating modes; privileged and user mode. Change between
these 2 modes should be done with care.
Clear the SR.MD bit to change from privileged mode to user mode, and use
an exception request to change from user mode to privileged mode.
After reset SH-3 executes programs in privileged mode in P2 area. If you
change from privilege mode to user mode with a P2 area address, it will
cause an address error. In other words you’ll have to have a U0 area
address and then change to user mode. Execute the RTE instruction after
setting SPC and SSR to those conditions.
To return to user mode from the called privileged mode, use the RTE instruction.
The SR.MD=0 condition that was saved to SSR is restored and it becomes user
mode. |
|