| 6-6 29-bit Address Mode and 32-bit Address Extended
Mode |
  |
The SH-4A can use 32-bit address mode.
32-bit address extended mode is set by setting the SE bit of the Physical
Address Space Control register (PASCR).
The maximum physical address space is 512 MB in 29-bit address mode,
but in 32-bit address extended mode, the P1, P2 areas can be mapped anywhere
in a 16MB to 512MB space using the 16 entry privileged space mapping buffer
(PMB).
|