| 13.9 Connecting CPU to Memory (16-bit Data Bus) When connecting a CPU and a memory using a 16-bit data bus, use a pair of memories having 8 bits per address, or use a memory having 16 data pins. The example described here uses a pair of memories having 8 bits per address, which are connected as memories at even- and odd-numbered addresses, respectively. To read/write 16-bit data, two addresses must be accessed simultaneously. It is impossible, however, to output two addresses to the address bus simultaneously. Remember that the upper digits of 16-bit data in the memory must be stored in an even-numbered address and the lower in an odd-numbered address (even-numbered address + 1). An "even-numbered address" and an "even-numbered address + 1" are the same from A23 to A1 in binary notation and only A0 differs. No problem arises if A0 is not used, since A1 to A23 are the same. A0 = 0 represents an even number and A0 = 1 an odd number. A combination of an "odd-numbered address" and an "odd-numbered address + 1 (even-numbered address)" does not make A1 to A23 the same, disabling access as 16-bit data. This situation is not limited to the H8/3048 but common to all 16-bit microcomputers. HWR and LWR are used instead of the A0 signal. HWR = L represents 8-bit writing to an even-numbered address (A0 = 0) and LWR = L means that to an odd-numbered address (A0 = 1). HWR = LWR = L means writing to both even- and odd-numbered addresses. Only the RD signal is used for reading by the CPU. During reading, data are always handled as 16 bits without distinguishing between 8- and 16-bit data. Sixteen bits are read even if the MOV.B instruction is used for reading from the memory. Non-used 8 bits are not read into the CPU although they are output from the memory. Reading data not required for the memory will not have a negative effect. For writing, however, 8- and 16-bit writing must be clearly distinguished since it changes the contents of the memory. This is shown in Table 13.10.
Figure 13.27 shows an example to connect the CPU and SRAMs using a 16-bit data bus.
| ||||
| The capacity becomes 1Mbyte since two SRAMs are connected and the addresses are between H'100000 and H'1FFFFF since CS0 = 0 and A20 = 1. Address, CS and OE signals are commonly input to two memories. For the memory at an even-numbered address, HWR is input to the WE pin and the data pins are connected to the upper 8 bits of the CPU. As for the memory at an odd-numbered address, on the other hand, LWR is input to the WE pin and the data pins are connected to the lower 8 bits of the CPU. |