| 在AV产品数字化不断加速的过程中,先进的细微化工艺技术发挥了巨大的作用,但是,在实现节省功耗方面,有时会面临较大的困难。为了解决这个问题,在这里推荐了几款最佳的瑞萨MCU。此外,数码AV产品的开发到上市的生命周期非常短,大约只有1年,因此,由子MCU实现最终产品的未定规格、差别化及附加功能怎么样? |
|
从瑞萨丰富的MCU产品线中,推荐3大Tiny系列作为子MCU。R8C/Tiny和M16C/Tiny由于是同一体系结构的系列,根据需要实现规格的规模,能轻松向高位型号或低位型号转化。并有着从20引脚到80引脚的丰富产品线。H8/Tiny由于是小型高功能MCU的第一系列,作为通信功能充实的产品而推荐给大家。 |